NEW: Quick Detach Sling Swivels from Halder for rifles with third-party sockets
Quick and quiet attachment and detachment of rifle slings
The rifle sling is just as indispensable as it is troublesome in many situations. This is why the task of attaching and detaching the rifle sling should be nothing more than a five-finger exercise. The feature that makes it exactly that is the PUSH & GO Sling Swivel from Erwin Halder KG. The new QD version for precision rifles made by Erwin Halder KG now also ensures compatibility with most rifles world-wide.
Precision rifles are available for a wide range of purposes, such as hunting, sports or security. Efficient and ready for use quickly in a great many applications, they are also highly favoured by marksmen thanks to their exceptional precision. The system that has become the established solution around the globe in terms of, for example, quickly removing the rifle sling from the weapon is the Quick Detach (QD) system. The new PUSH & GO QD Sling Swivel for precision rifles has been designed precisely to complement this system.
“Until now, our PUSH & GO Sling Swivels worked only in combination with Halder sockets. While forming the perfect match with these sockets, their compatibility was limited - especially when it came to other sockets on the international market,” explains Bernd Janner at Erwin Halder KG. “This is why we have decided to offer our QD version for precision rifles as well. This allows it to fit into most third-party sockets. This new solution allows for the effortless use of our PUSH & GO Sling Swivels on precision rifles used around the globe.”
The new version has not changed the way the product works: The connection between swivel and socket can be severed with the press of a button, allowing you to detach the rifle sling quickly and easily – and without any noise: The plastic-mounted balls incorporated between swivel and socket reliably keep the swivel from squeaking while being rotated. The quality of production is still guaranteed by the “Made in Germany” seal. The use of non-rusting materials makes all PUSH & GO Sling Swivels exceptionally good choices for outdoor use – even in rain and snow.
To learn more about the PUSH & GO Sling Swivels, refer to the information and videos on their quality and craftsmanship provided at https://push-and-go.eu.
The new QD PUSH & GO Sling Swivel of Erwin Halder KG is now also compatible with third-party sockets.
The QD PUSH & GO Sling Swivel turns the task of removing and attaching the rifle sling into a simple five-finger exercise - everywhere in the world.
Downloads: