EH 23220.
您的选择导致 1 打击
More details
外壳
本体
为了安全运行,螺纹孔M 12必须一直关闭。
固定于夹板 23210.0740,可有额外灵活的可能性。
M8规格的螺纹销可以固定于各种定位销和支撑座如 EH 22...。客制化延长版本也可以固定。
夹合高度可以使用高度调整圆柱 EH 23310,以及间隔片 EH 1107 和 EH 1108 来增加。
组装和设置:
固定支撑组件 (2 x M 6 thread) 在装置上。 注意操作者那侧!
替代方法:拆下M 12×10螺纹销更换成一个M12×30螺纹销和用钣手来装配支撑组件(WS21),即T型槽装配(没有明确的操作员一侧保证)。螺纹销M12×30和T-DIN螺母508 M 12×14,质量10,是标准供应量的一部分。
通过16毫米降低支撑组件是可能的。
夹钳過程:
含铅 - 符合例外 6a / 6b / 6c
含铅 - SVHC [REACH] 清单截至 2024 年 1 月 23 日
铅暴露会导致癌症和生殖伤害
https://www.P65Warnings.ca.gov/
„本产品不含来自刚果民主共和国或邻近国家的任何被指定为“冲突矿物”的物质,例如钽、锡、金或钨。
The supporting element can provide additional support at overdetermined clamping points, e.g. on unstable components. It helps reduce vibrations and damage to the surfaces during processing. This improves the surface quality of the workpiece and the service life of the tools dramatically.
The contact force ranges between approx. 20 and 70 N.
The supporting element can also be manufactured as a custom version with a different contact force. You are welcome to send us your request if you require such a version.
Since the surface is not covered by a clamping claw, it is possible to work on the top and the side surfaces.
The bedding support may be a good and cost-effective alternative. A poor and unprofessional option is the so-called screw jack, also referred to as a “slacker”.
Here, it is essential to factor in the necessary torque (15Nm). It may not be possible to apply the necessary torque with a hex wrench and T-Handle.
Repairs are possible in most cases. To arrange for repairs, please contact our sales department.
The supporting element is maintenance-free and does not have to be subjected to special servicing. We do, however, recommend that you regularly perform visual inspections and function tests. You should also pay attention to the oil concentration in the cooling emulsion as the functional parts on the interior may otherwise sustain corrosion.
Contact Form
News
Have a look to our current new parts:
Locating Pins Eccentric Clamping Clamps Pitbull® Clamps Centering Clamping Mandrels