EH 23340.
由于横向的处理也可以用于盲钻孔。
用于夹紧和居中的工件与内孔。
The centering clamping mandrels have the following characteristics:
您的选择导致 1 打击
More details
本体
夹持螺丝
定心夹紧心轴可以加工到所需的座直径(例如通过车削/铣削)。必须注意的是,在加工定心夹紧心轴之前, 在夹紧直径上0.1毫米。为了加工心轴,将提供一个锁定环。
The internal hexagon, which is attached to the side, allows the outer diameter to be expanded.