EH 25163.
Hinges from zinc die-cast with spring return allow doors to be automatically opened or closed.
The torque of the reset depends on the opening angle of the hinge (refer to the drawing). Endurance tests have shown that the torque of the reset does not change even after 100,000 cycles.
These hinges from zinc die-cast are characterised by their simple and timeless design.
您的选择导致 4 打击
More details
本体
弹簧
复盖
符合指令 2011/65/EU 和指令 2015/863
不含超过 0.1% w/w 的 SVHC 物质 - 截至 2024 年 6 月 27 日的 SVHC 清单.
不包括 65 号提案物质
https://www.P65Warnings.ca.gov/
„本产品不含来自刚果民主共和国或邻近国家的任何被指定为“冲突矿物”的物质,例如钽、锡、金或钨。